AnsweredAssumed Answered

AD9979 IC testing

Question asked by maheswariamudha on Apr 26, 2017
Latest reply on Oct 19, 2017 by 阿衡Irene

I want to test the AD9979 IC by giving the 27MHZ sine wave signal as the input to CCDINP instead of CCD signal from the camera. Serial write is done as per data sheet (pg.no 36) example register settings for power up . CLI is given as 27MHZ signal . Then HD signal is 23 KHZ and VD signal is 60 HZ signal generated as per data sheet pattern. I want to receive the D0-D13 siganls corresponding to my input signal . Is it possible to test in this method . Is there any evaluation kit is available for programming AD9979 and testing it.

Outcomes