AnsweredAssumed Answered

The transmit power of AD9361 is less than normal

Question asked by WXS on Apr 25, 2017
Latest reply on May 4, 2017 by Vinod

Hello everyone

When the AD9361 transmits a single carrier signal, the transmit signal is attenuated to 7db. Tested the power of the transmitted is 4.6dbmmy PCB board have a 15dB amplifier, and that is smaller than the power value in the normal case . I have modified the frequency word register, the RX gain table register, the BB DC and RF DC calibration register, the TX Quadrature register, the Transmit power register. SO, In addition to the above registers, which AD9361 registers also have effect on transmit power?

Outcomes