AnsweredAssumed Answered

Need an envelope detector working at -55C

Question asked by sinan.onat on Apr 21, 2017
Latest reply on May 11, 2017 by sinan.onat

Dear Staff and fellows;

I need an envelope detector working at -55C. My frequency of operation is 60 +/-3 MHz. I was hoping to use ADL5910, but I was guided -by sales representative- as I can not use ADL5910 IC for envelope detection.

Then the choices are left as ADL5904, HMC1120, ADL5511, HMC1030 and HMC1021. I need a guidance now on which one to use. Please share any useful information -especially on the operational temperature- about these ICs.

To complete my requirements, let me list that:

- I use 5962-9864601QEA in front of this envelope detector, so the input range should be compatible with the output range of 5962-9864601QEA.

- I need an operational temperature range of -55C to +85C.

- My operational frequency is 60 +/- 3 MHz. However I want an envelope detection of 1 MHz window.


Sinan ONAT