AnsweredAssumed Answered

AD9152 DC Test Mode Configuration

Question asked by on Apr 20, 2017
Latest reply on May 23, 2017 by larrywelchusa



I want to run AD9152 in DC Test Mode. For this do I need to follow all the device setup steps i.e. steps 1 to 5 mentioned in data sheet? Or is it sufficient if I just start up the DAC and do physical layer setup i.e. step 1 and step 4 and then just configure the registers for Digital Modulation, DC offset and DC test mode?


I want to test the DAC without providing external digital data input through JESD204B lanes. I am planning to generate a sine wave conbining Digital Modulation (fdac/8 modulation) and DC offset.


If you can provide me with the list of registers that are to be configured for running AD9152 in DC Test Mode that will be very helpful.