AnsweredAssumed Answered

INTERRUPT HANDLER ERRORS

Question asked by @~rakesh on Apr 20, 2017
Latest reply on Apr 26, 2017 by Jithul_Janardhanan

HI,

we are using the custom target board BLACKFIN ADSP-609. Till now we are using TWI interrupt in core0 now need to   shift  to core1.

problem : when the interrupt occurs the following error is displaying.
A fatal error or exception has occurred.
  Description:   No dispatched handler available for the specified interrupt code.
  General Type:  RunTimeError
  Specific Type: NoDispatchedHandler
  General Code:  0x8
  Specific Code: 0xb
  Error Value:   0x001b0020
  Error PC:      0xffa013ca

Please suggest how to fix it.

Regards.
Rakesh

Outcomes