AnsweredAssumed Answered

AD9371 with ZC706, booting linux

Question asked by adgoodw on Apr 19, 2017
Latest reply on Apr 19, 2017 by adgoodw

Hi,

I posted in the FPGA  reference design forum but seems like my issue is more appropriate here.

 

As above I am using D9371 and ZC706 and now would like to boot manually without TES and shipped SD card. From the information I gathered on these forums I take it that I should be using HDL and Linux 2016_r2 branches. Is this correct? I am following instructions here: https://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq .

I used the zynq-zc706-adv7511-adrv9371.dts device tree, and for uboot I used the u-boot-zc70x.elf from the SD card bootgen_sysfiles.tgz folder.

 

Linux does not boot, but I see activity on the UART, which stops at **Unable to read file uramdisk.image.gz**. Is there some obvious step that I am missing or did wrong?

 

Thanks,

Outcomes