AnsweredAssumed Answered

AD9957 Single Tone Initialization via FPGA

Question asked by creed on Sep 29, 2011
Latest reply on Mar 15, 2013 by KennyG

I'm trying init the AD9957 using an FPGA.  So far I've been unsuccessful.  I believe

the timing of my SPI inerface is correct, but I'm not sure that I'm doing everything

that needs to be done to generate a single tone.

 

Attached is the timing diagram from my design.

 

During ad9957_rst the SPI bus sends out a read instruction.  I don't look at the SDO

line, I just have it issuing a read to make sure that I don't write to a register accidently.

 

After reset I issue a write to Register 0x14 which I think is a 64 bit register.  The next

4 bytes are each 0x00 which covers the scale factor and phase offset word.  The next 4

bytes are each 0x33 which is a frequency tuning word.

 

After that I assert PS1 so that PS is now 110 which I believe is a Single Tone profile.

Asserting one of the PS lines should generate an internal IO_Update which should

initializae the device.

 

I also assert spi*_cs and kill spi*_sck to prevent any additional writes from occurring.

 

Is this an appropriate way to generate a tone with the AD9957?

 

Things I've checked:

 

The board works with the evaluation software

The signal levels look clean

 

Regards,

Attachments

Outcomes