AnsweredAssumed Answered

AD9371 API

Question asked by JTANITA Employee on Apr 13, 2017
Latest reply on May 17, 2017 by gverma

A customer asks:

 

I am trying to work with the ADI provided API for the AD9371, but I have encountered an issue that I am having trouble resolving.

 

Background:

  • I am running Vivado and XSDK 2016.4 on Windows 10
  • I built the provided HDL for the AD9371 and exported to SDK
  • I imported all of the API source code into a new project in XSDK
  • I am using common.c/h without any modifications
  • I am using the auto-generated headless.c/h files for a sample application (which I will customize later)
  • For now, I created stub code for the drivers that I am developing (because we have chosen to run bare metal, No-OS)
    • This temporarily resolved issues with spi.h, logger.h, and others not being defined

 

Current Problem:

  • When I try to build the API (with my “stub code”) I get the following error:
    • Error à undefined reference to nanosleep in common.c
    • This function is used within the function CMB_wait_ms()
  • This function appears to be defined in time.h which is included in common.c
  • Additionally the POSIX extension should be enabled in common.h with #define _POSIX_C_SOURCE 199309L

 

Can you please advise on how I can resolve this issue?

Outcomes