AnsweredAssumed Answered

Can we use adi_rom_boot() on ARM to boot SHARC cores 1 and 2 ?

Question asked by anupsk on Apr 12, 2017
Latest reply on Apr 25, 2017 by nithya.koch

I am using SC584 board.

I want to create 3 different ldr files for each of the core so that I can place them in non-contiguous  memory locations in SFLASH. If I do this, I believe BOOTROM would not take care of loading all the binaries as they are not contiguous and BOOTROM would be loading only ARM binary. Then I need to use adi_rom_Boot() in ARM application to load binaries for SHARC 1 and SHARC 2.

 

Can I use adi_rom_Boot() on ARM to load binaries for SHARC 1 and 2 ? Or is there a easier way to load binaries if I am placing them in non-contiguous locations in SFLASH ?

Outcomes