AnsweredAssumed Answered

ADUCRF101 - Preamble settings

Question asked by adrianchia on Sep 29, 2011
Latest reply on Sep 30, 2011 by PatrickN

Hi All,

 

I will like to find out if ADUCRF101 can support the below following :

 

1.     ADUCRF101 has a fixed preamble sequence of 0x55. Can we customised it to something else like 00110011 or 10101010 etc?

2.    The preamble length can support up to 255 bytes which is typically in the range of a few tens to hundred ms range. Can we further extend it to 1s or even up to 60s as we have some unique energy saving protocol to implement ??

 

Thanks for the help in advance!!

Outcomes