AnsweredAssumed Answered

Can AD9162 use FIR85 when JESD M=1?

Question asked by GRL on Apr 12, 2017
Latest reply on Apr 19, 2017 by danf

Would like confirmation that AD9162 can be used as follows: 

JESD mode :  L = 8, M = 1, F = 1, S = 4. 

Lane-Rate = 12.5 Gbps/lane

5.0 GHz into DAC-Clock (CLK+, CLK−) 

2x NRZ interpolation, for image suppression

FIR85 runs at 10 GSa/sec complex

DAC update @ 10 GSa/sec 

Output = real signal from DC to 2.25 GHz (45% of 5.0 GHz)

 

I'm not 100% confident, from reading the datasheet ... much of the description is for M=2 modes.

Thanks!

Outcomes