AnsweredAssumed Answered

AD9164 Full performance Configuration

Question asked by Karthik_FAE on Apr 11, 2017
Latest reply on Apr 28, 2017 by danf

We are evaluating AD9164 High Speed DAC and want  to try evaluating the part up to 6 GHz output.

As mentioned in the Datasheet, DC to 6 GHz in 2× nonreturn-to-zero (NRZ) mode. How can we set these settings in ACE and by using ADS7? Is NCO only configurable through SPI or it also can be configured via JESD?

Outcomes