AnsweredAssumed Answered

HMC1099 Eval Board - where can I source an inductor like "L2", which is a 900nH (0.9uH) case size 1008? All I can find have SRF of around 470MHz, surely these will make the HMC1099 oscillate?

Question asked by meyrick on Apr 11, 2017
Latest reply on May 3, 2017 by meyrick

I wish to use this value of inductor as it clearly gives the HMC1099 its widest frequency range capability, so where did Analog Devices Inc get this inductor? Has it also a SRF within the HMC1099 frequency range of operation? Perhaps it isn't a problem?

Any ideas, thoughts or help would be much appreciated.

Outcomes