AnsweredAssumed Answered

Fluctuations in Current Channel Under No Load

Question asked by mamech on Apr 7, 2017
Latest reply on Apr 24, 2017 by nchandra

Hello

 

I am using ADE7953, and I noticed that the current reading suffers fluctuations in range of around 2mA to 9mA when the load is unplugged. Is there any thing that I can do to make the no load current to be stuck at some known level ? I thought about connecting 5 mega ohms in parallel with load so when load is unplugged the current stays at known level. I do not know if this is a good idea or not.

 

 

attached the schematic of shunt circuit

 

 

Outcomes