AnsweredAssumed Answered

DC voltage follower with AD623

Question asked by aadd623 on Apr 5, 2017
Latest reply on Apr 6, 2017 by aadd623

Hello there,

 

I'm trying to build a DC voltage follower with AD623ANZ. When INPUT = 0 V, OUTPUT=0V which is fine. But when INPUT=3.4V, OUTPUT=1.7V which is disappointing. So it's not following. Can someone take a look at the attached circuit diagram and tell me why this doesn't work? Thanks much.

Attachments

Outcomes