AnsweredAssumed Answered

How to add the AD9361 Linux driver on Petalinux

Question asked by ramon.righini on Apr 5, 2017
Latest reply on Jan 8, 2018 by ramon.righini

Hello,

 

I need to add the AD9361 Linux driver on Petalinux 2016.4 for a project with Xilinx Zynq Ultrascale.

I can't change our kernel with the Analog Devices one, so if I understood well (from the other forum posts), I must build a kernel module of the mentioned driver. Is it correct?

I'm new on Linux, and probably my question is dummy: what are the involved files to build the kernel module of the AD9361?

Further, the ".dtsi" file is the initial configuration of the device with the Linux driver. Can I use the same method to initialize the AD9361 also if I will implement a kernel module?

 

Thanks and Regards

Outcomes