AnsweredAssumed Answered

(ADuM14x)Can you check the Pin status ?

Question asked by donadona999s on Apr 4, 2017
Latest reply on Apr 4, 2017 by donadona999s

Hi !

I have some questions about ADuM142.

Can you check that my understanding are correct or wrong?

 

This is the circuit from my customer.

When they are using under the condition "status 1" , IC2 VOC depends on VIC because IC2 VDD1 = VDD2 = VE1 = 5V.

 

Also this is another condition.

Ic2 VDD2 = 0V.

So it will move to default status.

Our customer are using "ADuM142E1WBRQZ-RL7" so VIC output will be "H".

 

Is my understanding correct?

 

Best regards

Kawa

Outcomes