AnsweredAssumed Answered

ADV7343- P_BLANK# Pin

Question asked by emilzacharia on Apr 3, 2017
Latest reply on Apr 4, 2017 by emilzacharia

Hi,

I'm using ADV7343 to encode the 24-bit RGB signals to analog CVBS signal. Is it fine?

 

I have only the following signals as shown in the diagram from the bridge.

I've connected the RGB data signals, HSYNC, & VSYNC signals to ADV7343.

 

Is that enough.

Should I connect some signal to the P_BLANK # input?

Or, leaving it float be fine?

 

Please do help.

 

Thanks in advance.

Emil Zacharia George.

Outcomes