AnsweredAssumed Answered

ADXL 377 behavior with g-force maxed out.

Question asked by asinopoli66@gmail.com on Mar 31, 2017
Latest reply on Apr 21, 2017 by John.Tuazon

While using a very accurate military grade force sensor we measured 180 g's and 193 g's on respectively on 2 devices. 

 

We then added the ADXL377 in an area that should give us higher g force number and saw numbers in the area of 14-20 g's.

 

So we are wondering of this may be 214-220g's or if they are just random numbers because we maxed out the 200 g performance threshold of the ADXL377?

 

Thoughts/feedback appreciated.

 

Tony Sinopoli

Outcomes