AnsweredAssumed Answered

is ADV7511W TMDS output is 8b/10b format

Question asked by tramesh2706 on Mar 27, 2017
Latest reply on Mar 30, 2017 by tramesh2706

The ADV7511W output to DVI monitor in 1024 X 768 resolution , the monitor continuously in ON condition but it is not displaying the video pattern. I am driving the ADV7511W from FPGA with 24 bit RGB data with separate sync and DE signals.  I am using 24 inch dell monitor. monitor in ON condition only with this resolution, with other resolution it goes to sleep mode and again comes back to ON and goes to sleep this cycle continuous. in 1024 X 768 resolution it is continuously ON condition but not displaying video, also monitor control  buttons are not working in this condition

Outcomes