AnsweredAssumed Answered

Maxing out the volume ADAU1701

Question asked by danny08 on Mar 24, 2017
Latest reply on Apr 6, 2017 by danny08

hi,

im using a adau1701 as a controller for my private public adress system.

Also im using a bluetooth device as input but i'm not very happy with the maximum volume, i dont think i got the full 0,9v rms output for my amplifier.

Is there a way to auto detect the maximum or maxing out the volume without getting into clip depending on the input?

or should i just use +20db max gain and then put a single slew ext vol after it and "detect" the clip by my ears?

greetings

Outcomes