Rob.Analog

How Does the Free-run Mode Work in the ADV728x Devices ?

Discussion created by Rob.Analog on Mar 24, 2017

The post is valid for the ADV7182, ADV7280, ADV7280-M, ADV7281, ADV7281-M, ADV7281-MA, ADV7282, ADV7282-M and ADV7283.

 

How Free-run Works

Free-run mode is a mode where the ADV728x ignores in incomming analog video input and outputs a test pattern. The ADV728x device has a line based FIFO memory block in the digital core of the part. Usually this store about 3 to 5 lines of active video ( i.e. video that's been output by the ADC in the ADV728x).

However there are also a few test patterns stored in the FIFO memory block. In free-run mode the active video lines are ignored and the test patterns are output instead. The test patterns consist of a single line that is repeated over an over again to create a full field.

By default the ADV728x will output a blue field however It is possible to modify the output color or select a number of different test patterns. See the  "FREE-RUN OPERATION" section of the ADV7182 datasheet and ADV728x hardware manual for more information.

http://www.analog.com/media/en/technical-documentation/data-sheets/ADV7182.pdf 

http://www.analog.com/media/en/technical-documentation/evaluation-documentation/ADV7280_7281_7282_UG-637.pdf 

 

When ADV728x Enters Free Run

By default the ADV728x will enter free-run mode if it is not able to connect to an analog video source. Using standard scripts, after an analog video source is disconnected it can take the ADV728x upto 1 second to enter free-run mode. Using Fast Swtiching scripts it can take the ADV728x under 250 ms to enter free-run mode. For automotive applications analog devices advises using fast swithcing script. See this post for more information on Fast Switching script. Fast Switch Mode- ADV728x 

 

It is also possible to force the ADV728x not to enter free-run mode if a source is disconnected. Setting the  "DEF_VAL_AUTO_EN" bit (user map register 0x0C bit [1]) will force the ADV728x not to enter free-run mode if a source is disconnected. This mode is not advised as the ADV728x will output noise until a black noisy video source is connected. 

 

What Format will the ADV728x output in Free-Run Mode

See this post for more details What Video Output Standard does the ADV728x Output in Free-Run Mode 

 

Non-standard field length

 

It is possible for the ADV728x to output fields that are too long/ short. See this post for more details. 

https://ez.analog.com/message/295118

Outcomes