AnsweredAssumed Answered

How to connect ad5761

Question asked by renato62 on Mar 23, 2017
Latest reply on Mar 23, 2017 by clon

I would use "AD 5761" to have a 0-10V output Vout.

I have to obtain an output voltage from 0 to +10V, having available voltages of +24V, +5v and 3,3V.

 I have only SDI, SDO, SCK and SYNC signals (as MOSI, MISO,  SCK and SS of a microcontroller).
I would link /LDAC to Gnd and /CLEAR to Vcc.

I enclose file in .pdf format ad I would link the ad5671.
I have the microcnotroller inputs at +3.3V.
I'm not sure I have connected in the circuit diagram the correct voltages.
Can Someone help me?
best regards
Renato

 

Outcomes