AnsweredAssumed Answered

cn0229 not connecting via SDP-H1?

Question asked by EricTPG on Mar 21, 2017
Latest reply on Mar 23, 2017 by EricTPG

I'm using a SDP-H1 (rev 1.3) platform with a CN0229-SPDZ (Rev A) and an EVAL-AD7761FMCZ (Rev. A).  If the CN0229-SPDZ is the only thing connected to the SDP-H1 it is recognized by the CN0229 application.  If the EVAL-AD7761FMCZ is connected though, the CN0229-SPDZ is not able to be found by its application (the AD7761 Evaluation Software works fine).

 

I'd like to work with both of these systems at the same time from a single host/power source (eventually).  Is there a way to make this work or is there something inherent that will prevent this?  (SPI not daisy chained or addressing collisions or some such?)

 

Thanks,

Eric

Outcomes