AnsweredAssumed Answered

ADSP 21489 JTAG Connector Debug Agent

Question asked by Mildocate on Mar 20, 2017
Latest reply on May 30, 2017 by Jithul_Janardhanan

Hej all,

 

I am creating my own board with the ADSP-21489 with 176 Pins. 

I have the EZ Kit with Stand Alone Debug Agent.

On the board are two connectors JTAG P1 and ZP1. For the P1 I know the connections to the DSP from the schematic. But the ZP1 is not included in the schematic. How are the pins of ZP1 connected to the DSP?

 

I measured the following:

1   5 V supply

2   5 V supply

3   NC (?)

4   3.3 V supply

5   NC (?)

6   Reset

7   NC (?)

8   DA Soft Reset

9 -14  GND

 

Is this correct?

 

Second:

In the EE-68 document Pin 1 is connected to GND but on the EZ Kit its 5V. 

So I also have to route Pin 1 to 5V?

 

Thanks!

 

Waleri

Outcomes