AnsweredAssumed Answered

Availability of ADF4159?

Question asked by jsaily on Sep 26, 2011
Latest reply on Sep 30, 2011 by enash

Can someone from ADI confirm when the new ADF4159 will be available? I noticed from the ftp site that there is a preliminary datasheet along with the Frac-N v3.5 software. Max PFD seems to be 110 MHz which is very good for fast FMCW ramps. Possible problems could be caused by the 3.3V max charge pump voltage (5.5V with ADF4158).

Outcomes