AnsweredAssumed Answered

DAC Requirement

Question asked by Maria Employee on Mar 14, 2017
Latest reply on Mar 15, 2017 by msamera

WE NEED THIS CONVERTER FOR OUR DC SERVO MOTOR.THERE IS ONLY PULSE CORDER ARE INBUILD IN THE MOTOR. DRIVE NEED TACHO SIGNALE IN +-10V FOR POSITIONING . BECAUSE DRIVE IS ANALOG . WE WANT TO DO PULSE CODER SIGNAL SEND TO DA CARD AND CARD OUT PUT -10TO +10V SEND TO DRIVE . DRIVE CONTROL THE RPM. OUR PULSE CODER IS 2500P AND MOTOR MAXIMUM RPM IS 2000. WE WANT AT FORWARD 2000RPM DA CARD SEND OUTPUT +6V AEVERSE 2000RPM DA CARD SEND OUTPUT -6V. PLEASE SUGGEST ME IF ANY PRODUCT SUITABLE FOR ME

Outcomes