AnsweredAssumed Answered

AD9834 Eval Board Comparator Output does not change with analog output change

Question asked by GabrielKRS on Sep 23, 2011
Latest reply on Sep 27, 2011 by LiamR

Hello,

 

     I am trying to use the AD9834 to output a square wave output by way of the comparator. I am using the Blackfin SDP board connected to a Windows XP PC and the AD9834 software provided with the evaluation board to control it.

     No matter what the analog output value is set to (so far I have tested 0MHz, 5 MHz, 10 MHz, 12 MHz and 15 MHz), the comparator always outputs a 10 MHz square wave. I do not know what could be causing this problem, as I would expect that a change in the Vin being fed to the comparator would make a change in the comparator output. I can give more information about my setup on request. Any help is greatly appreciated.

 

-Gabriel

Outcomes