AnsweredAssumed Answered

AD5760 Supply Range

Question asked by RBeen on Mar 9, 2017
Latest reply on Mar 15, 2017 by msamera

The AD5760 datasheet indicates that Vdd can be as high as 30.5V with Vss being -2.5V. This falls within the listed absolute maximum ratings, however the pin descriptions and other product literature indicate that Vdd and Vss are +/- 16.5V. Would the device still function correctly given Vss of -3V and Vdd of +28V? Thanks for your help in advance.

Outcomes