AnsweredAssumed Answered

AD80066 clocks

Question asked by pixelPhile on Mar 9, 2017
Latest reply on May 5, 2017 by pixelPhile

I'd like to use the AD80066 to digitise the outputs of 4 CCD channels whose maximum clock rate is 1MHz (each).  In many ways the part is perfect if it can run that slowly (ADCLK @ 4MHz).  The datasheet does not indicate any minimum frequency or maximum period, but there are suggestions elsewhere on EZ that there is a minimum frequency that should be observed.  If so, what is it?

 

If the 80066 is not suitable, can you suggest a part that would be?

 

I'd really appreciate a definitive answer from an AD staff member!

Outcomes