AnsweredAssumed Answered

LDO Charger

Question asked by stillli on Mar 8, 2017
Latest reply on Mar 23, 2017 by jstaley

1. EVAL-AD8450 is a switching charger. Can I set the charge current to linear constant current (no ripple)?

  Can I programm the current in one charge cycle? (0.1A before 2.5V, 2A 2.5-4V, 1A 4-4.2V)

 

2. Need one LDO charger,

a. Programm output voltage: 4.9 V max

b. Similar with EVAL-AD8450. evaluation board, front end with current sensor

c. Programmble charging current, like pules: 1-2ms: 0.9A,  2-4ms:1.1A......

 

Than you 

Outcomes