AnsweredAssumed Answered

SigmaStudio CCES not a valid tool-chain on Win 10

Question asked by toani on Mar 7, 2017
Latest reply on Mar 8, 2017 by toani

When I open a project in SigmaStudio, I get the following message:

 

Error when opening a project in Sigmastudio on Windows 10. CCES 2.5.0 was previously installed.

 

CCES does not appear in settings where I have seen is on other machines.

Settings menu

I am using windows 10.

Is there a solution to this?

I cannot compile nor run. Here is the error.

Link

Output

 

Additionally, if I try to create an algorithm with Algorithm Designer from SigmaStudio for Sharc, this is what I get when I try compiling the algorithm. I assume the root cause is the same of the problem above.

Generate assembly in Algorithm Designer, SigmaStudio for Sharc

Error compiling algorithm in Algorithm Designer from SigmaStudio for Sharc

 

Has anyone else have seen this error? Is there a workaround?

I am about to downgrade the OS to Win 7.

 

 

Thanks,

 

Daniel

Outcomes