AnsweredAssumed Answered

ADCMP607 comparator info

Question asked by Ansar on Mar 6, 2017
Latest reply on Mar 16, 2017 by rrosario

Hi,

 

We are using ADCMP607 comparator one of our design.
Please provide below info for my design.

1> Can we connect same power supply voltage to both VCCI and VCCO or connect the different voltages?
what is non operating range in electric characristics?
VCCI - VCCO Operating -3.0 +3.0 V
VCCI - VCCO Nonoperating -6 +6 V
Please elaborate.

2> Can i set hysterisis by just connecting one 100K or 200K ohm resistor pull down to ground to LE/HYS pin, if am not using Latch enable?.
In Figure 18. Hysteresis vs. RHYS Control Resistor graph
if i am connecting 100K pulldown then it show 100mV hysterisis. it means +/- 100 mV or +/- 50 mV?

 

3> we are using this comaparator in high speed paths where we need to measure 6 nS rise time of signal. How much delays the this comaprator add in signal path?

Waiting for reply..

 

Thanks and regards,

Ansar 

Outcomes