AnsweredAssumed Answered

HMC702 current of 3.3V

Question asked by tangke on Mar 5, 2017
Latest reply on Mar 8, 2017 by dyoung1

I'm thinking of using HMC702 and HMC1060 to build a phase lock loop.HMC702 is a quite great frequency synthesizer IC and HMC1060 is a LDO which can produce one 5V 300mA,two 3.3V 50mA and one 3.3V 100mA in one IC.In HMC702's datasheet ,it says that +3.3V,VCCPRS,RVDD,VCCHF 116mA,which should be separated to satisfy the output current of HMC1060.So,I want to know the precise current of VCCPRS,RVDD and VCCHF,so that I can decide how to separate?

Outcomes