AnsweredAssumed Answered

Run the AD9915 as if it had 1Hz resolution

Question asked by KevinF on Mar 3, 2017
Latest reply on Mar 3, 2017 by KennyG

I would like to produce exact 1Hz resolution frequencies (or power-of-2 divisors 1/2, 1/4, 1/8 Hz etc) while clocking the device at 2500MHz.    In Programmable Modulus Mode, can I set B to 2500e6, giving a modulus of 1.0737e19.   How do I solve for A and FTW to produce arbitrary frequencies between say 100 and 200MHz?

Outcomes