AnsweredAssumed Answered

EVAL01-HMC833LP6GE: Unexpected Reset Pulse when USB Module is detached. 

Question asked by Elker on Mar 3, 2017
Latest reply on Mar 23, 2017 by dyoung1

I have 2 evaluation boards EVAL01-HMC833LP6GE  and one USB Interface module. I'm trying to put both 833 boards in test simultaneously. But when I unplug the 833 form USB module a low pulse is sent to AD4, disabling the HMC1060, and the board resets, losing the configuration. i.e I can only operate the 833s with the USB module attached to them. 

There´s a way to avoid this reset pulse? Either at 833 eval board or at USB Interface module?

Outcomes