AnsweredAssumed Answered

EVAL-ADF7021DBZ5 for ADF7021

Question asked by Galih on Sep 21, 2011
Latest reply on Sep 21, 2011 by enash

Hi all,

I wanna ask about ADIsimSRD Design studio for Eval-ADF7021DBZ5.

 

Introduction:

- My team wanna make nanosatellite communication payload using ADF7021with the spec=
   Rx = 145.95 MHz (single channel with the width 10Khz)
   Tx = 436 MHz (width 30Khz)

 

- I have bought EVAL-ADF7021DBZ5 for my Rx requirement
     And then I use ADIsimSRD Design studio to get the output maching

 

 

Question=

I get the data sheet about ADF7021, and I see that there is EVAL-ADF7021DBX silkscreen, as my guidance to put my R,L,C components and make circuit for that evaluation board based on ADIsimSRD Design studio, but it's different R,L,C position name with the result that I get from ADIsimSRD Design studio. So, how to put my R,L,C components? Is there other  EVAL-ADF7021DBX silkscreen as my guidance?


Because
From SRD I get= L31, L32, L33, L33, L34, C31, C32, C33, C34, C35, C36

And in the data sheet, there aren't that component name

 

 

Thanks a lot for all of your help
I need the answer as soon as possible, thanks

Outcomes