AnsweredAssumed Answered

Have an AES-KCU-JESD-G  --       Need to run it with the latest version of Vivado (currently 2016.4),       Have updated and repackaged the Analog Devices IP  --  clock connections missing  [BD 41-758] The following clock pins are not connected to a valid

Question asked by mwilson@neptunetg.com on Feb 23, 2017
Latest reply on Feb 24, 2017 by CsomI

Have an AES-KCU-JESD-G  --
      Need to run it with the latest version of Vivado (currently 2016.4),
      Have updated and repackaged the Analog Devices IP  --  clock connections missing
 [BD 41-758] The following clock pins are not connected to a valid clock source:
/axi_ad9144_dma/fifo_rd_clk
/axi_ad9144_core/up_clk
/axi_ad9144_core/d_clk

How can I get these analog devices connections recreated in Vivado

Outcomes