AnsweredAssumed Answered

How do I program  AD9518-4 from ADIsimCLK?

Question asked by bjla on Feb 23, 2017
Latest reply on Feb 23, 2017 by pkern

I have updated the eval board software using AD9516_17_18_Evaluation_USB_Flash_Programmer.

I can communicate with the board using the AD9516_17_18_evaluation_software_full_install

I have manually installed the drivers on the computer so the board is identified as "ADI Evaluation System (LRFDev)"

BUT the "Program Chip" is grayed out.

 

I see that I should check that the ADIsimCLK actually supports the board in question but I have no idea of where to find such information.

Outcomes