AnsweredAssumed Answered

Issue- Flash U-Boot to SPI Flash  via Ethernet

Question asked by svs on Feb 22, 2017
Latest reply on Feb 23, 2017 by svs

Hi all,

                      I'm working on CCES 2.3.0 linux version, When I try to Flash U-Boot via Ethernet I got the Following Issue

 

 

U-Boot 2015.01 ADI-1.1.0 (May 30 2016 - 14:25:12), Build: jenkins-IP119-UBOOT-STAGE-DEB-label=make_d8

CPU: ADSP ADSP-SC589-0.0 (Detected Rev: 1.1) (spi flash boot)
VCO: 450 MHz, Cclk0: 450 MHz, Sclk0: 112.500 MHz, Sclk1: 112.500 MHz, DCLK: 225 MHz
OCLK: 150 MHz
I2C: ready
DRAM: 224 MiB
MMC: GRIFFIN SDH: 0
SF: Detected W25Q128BV with page size 256 Bytes, erase size 4 KiB, total 16 MiB
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
other init
Net: dwmac.3100c000
Hit any key to stop autoboot: 0
sc # dhcp
Speed: 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 172.17.8.79 (4 ms)
sc # set serverip 172.17.8.144
sc # run update
Speed: 100, full duplex
Using dwmac.3100c000 device
TFTP from server 172.17.8.144; our IP address is 172.17.8.79
Filename 'u-boot.ldr'.
Load address: 0xc2000000
Loading: T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again
Speed: 100, full duplex

Outcomes