AnsweredAssumed Answered

CMOS logic as the output standard of AD9554

Question asked by miladmazi on Feb 21, 2017
Latest reply on Feb 23, 2017 by miladmazi

Hello,

 

I'm working with the EVAL-AD9554 board as jitter cleanup for my high-precision ADC (AD7760 with 24 bits). I was wondering if there is a way to get CMOS logic from clock outputs? Actually, I need 0 to 3.3 V clock to feed the AD7760. As I searched on the main web page for EVAL-AD9554 there was no documentation or application note about its configurations and that's why I'm confused. It would be highly appreciated if anybody can help me in this matter. Thanks 

Outcomes