AnsweredAssumed Answered

AD8564: input voltage

Question asked by Mr.K on Feb 20, 2017
Latest reply on Mar 29, 2017 by rrosario

Hello,

 

I have some questions about the absolute maximum rating of AD8564.

In the datasheet of AD8564, there is the following descriptions.

 

 

An analog power supply voltage describes 14V.

The input voltage describes ±7V.

Is the input voltage ±7V related to 14V of the maximum analog power supply rating?

 

I will use the power supply voltage of AD8564 in +10V single power supply.

In that case, is the maximum rating of the input voltage +10V?

Or, it +7V?

 

Best Regards,

Mr.K

Outcomes