AnsweredAssumed Answered

Last questions before purchasing the ADRV9371-W/PCBZ

Question asked by SDR on Feb 17, 2017
Latest reply on Feb 21, 2017 by Vinod

Dear All,

We are about to purchase the ADRV9371-W/PCBZ board and the ZC706 board.

Before ordering we have 2 questions about the Receive Bandwidth of the AD9371.

 We have a Rx only application.

  1. We have 2 different signals to demodulate one at 500 and the other at 800 MHz.
  2. Both of them have a 3dB bandwidth of 80 MHz and are QPSK modulated.
  3. We plan to filter and feed the signals to Rx1 and Rx2 seperately.

Question 1: Can AD9371 handle 80 MHz per Rx Channel?

 

Question 2: The JESD204 core is pricy. Do we have to purchase the core to make it work in ZC706?

 

Please confirm.

Outcomes