AnsweredAssumed Answered

AD8000&AD8001 PCB design issues

Question asked by coyoo on Feb 13, 2017
Latest reply on Jun 22, 2017 by coyoo

Hello,

 

I'm designing AD8000&AD8001 for testing purpose. The AD8000's datasheet says:"Do not use ground and power planes under any of the pins of the AD8000." Is this means that I have avoid copper of the ground (or power) plane adjacent top layer? 

 

Below is my baord's layers structure:(Do i have to remove some copper of the Agnd1 just under the AD8000&AD8001?)

And here is the AD8001 and AD8000 used in my new test board:

Anybody can show me an example of this?

Outcomes