AnsweredAssumed Answered

ADE9078 -ADC-

Question asked by Bastler on Feb 14, 2017
Latest reply on Feb 20, 2017 by Bastler

Hy, I have problem to understand the spec of the datasheet.

At page 5 is defined the differential Input range from -1V to 1V and in the next line is the maximum operating voltage from -0,6V to 0,6V.

Which value shall I choose ?

 

At Page 33 the voltage path is desribed, I didn't understand the values.

I thought the device use a 24Bit ADC, that means I have 2^24 = 16,777,216 bits

How do I get the different values for 1V at the analog Input,

sinc4 Output       : +/- 67,110,000

sinc4+IIR...         : +- 74,520,000

xV_PCF               : +/- 74,770,000

 

Kind regards

Outcomes