AnsweredAssumed Answered

HMC983 single ended input

Question asked by linhel on Feb 13, 2017
Latest reply on Feb 16, 2017 by linhel

Hi!

 

I'm planning on using the HMC983 as a programmable prescaler for the frequencies 200MHz to 6GHz.

Since I got such a wide input bandwidth I'm thinking of using one of the differential inputs as a single ended input as mentioned in the data sheet. I was just wondering if there are any example designs of this use case and if there is anything specific that I should think about or avoid when designing the input this way.

 

Thanks in advance!

 

Best regards

Outcomes