AnsweredAssumed Answered

ADAU1761: code generation

Question asked by Barricade on Sep 16, 2011
Latest reply on Sep 26, 2011 by BrettG

Hallo,

 

using the code generation (SigmaStudio 3.5.1, same with 3.5.3) show the following:

 

in *IC_1_REG.h

 

/* Playback Line Out Right  - Registers (IC 1) */
#define REG_PLAYBACK_LINE_OUT_RIGHT_ADDR          0x4026
#define REG_PLAYBACK_LINE_OUT_RIGHT_BYTE          1
#define REG_PLAYBACK_LINE_OUT_RIGHT_VALUE         0x0

 

in in *IC_1.h

 

/* Register Default - IC 1.Playback Output Signal Path Registers */
#define R10_PLAYBACK_OUTPUT_SIGNAL_PATH_REGISTERS_SIZE 14
ADI_REG_TYPE R10_PLAYBACK_OUTPUT_SIGNAL_PATH_REGISTERS_Default[R10_PLAYBACK_OUTPUT_SIGNAL_PATH_REGISTERS_SIZE] = {
0x21, 0x00, 0x41, 0x00, 0x03, 0x09, 0x01, 0x97, 0x97, 0xE6, 0xE2, 0x01, 0x00, 0x03
};

 

where 0xE2 is on the addr 0x4026.

 

Programming the DSP the value 0xE2 is used.

 

That means for me the output to *IC_1_REG.h is wrong on some places !

 

Best regards.

 

changed to correct addr

Outcomes