AnsweredAssumed Answered

MISS MUCH ADP505x_BuckDesigner_Release.xlsm

Question asked by OTI on Feb 9, 2017
Latest reply on Feb 16, 2017 by AIlustrisimo

I use ADP505x_BuckDesigner_Release.xlsm follow condition

 

 

 

and I got the fellow result.

Cout 13 4.7μF、Rc13=6.98K、Cc13=680pF

 

This value does not accord with the value of the equation of data sheet mention ((ADP5052,Page 26 NO3)

 

Data-sheets shows that 

 

I think that R=5Ω because R=5V/1A.

So Cc=5×4.7μF/6.98K

   ≒3.36nF

 

Is voltage dependence of a Cout13 considered by Excel calculation?

     

 

 

 

 

Outcomes