AnsweredAssumed Answered

HDCP on the ADV7619

Question asked by Glenn on Feb 9, 2017
Latest reply on Feb 12, 2017 by JeyasudhaMuthuPerumal

I am trying to get HDCP working on the ADV7619. I have tried both using the auto HDCP setting and manually setting to port B (which is the one we are using).  I also have the EDID RAM set-up and access enabled.  From HDMI Map 0x04, I read 0x20 (bit 5 keys read is set and bit 4 not set no error on HDCP Keys. Bit 3 is 0 which is calculated Ri has been read by TX source). Despite all of this I do not get valid video.

Outcomes