AnsweredAssumed Answered

Questions -2 for ADP5062

Question asked by Kaos on Feb 8, 2017
Latest reply on Feb 16, 2017 by Kaos

Dear Sir/Madam,

 

Our customer is studying with your ADP5062.
So I just got the following questions.

 

Q-1
When VINx=0v, ISO_Bx=2.3V to 4.2V,
can we put the 2.3V to 4.2V on DIG_I03 no prpblem?
Also can we put the 2.3V to 4.2V on SCL,SDA no prpblem?
Due to your ABS max ratings, it is no problem I believe.

 

Q-2
On your DS page-6, I can confirm Pull-Down Resistance.
So what is the recommended PULL-UP resistance value?
Same value of pull-down resistance, correct?

 

Thanks Kaos

Outcomes